Why set temperature isn't changing at the scheduled time. "Time zone" or "Summertime" is incorrect.
If radiator thermostat doesn't change set point temperature at the scheduled time, then you need to re-connect your smartphone with the internet access to the thermostat and new time will be updated via the internet automatically. If the issue remains the same, remove batteries from the thermostat or reset to the factory settings.