Can I use the thermostat without an App/Smartphone ?
Yes, if the thermostat haven’t been connected with an App, then it will operate as a standard thermostat. The set point in the display will be the temperature target. It is not possible to do schedule programming directly on the thermostat.